Cancel
Visit FS A global high-tech company providing high-speed communication network solutions.
https://media.fs.com/images/solution/gpon-ftth-access-network.jpg

FTTH Network Based on GPON

April 20, 2016

Why Is GPON Popular in FTTH Network?

GPON (Gigabit passive optical network) is defined by ITU-T recommendation series G.984.x. It can transport not only Ethernet, but also ATM and TDM (PSTN, ISDN, E1 and E3) traffic. It represents an increase in bandwidth compared with ATM PON (APON) and broadband PON (BPON). Supporting triple-play services, high bandwidth and long reach (up to 20 km), GPON can be applied in many scenarios especially in FTTx networks. Besides, GPON customers are typically homes or small businesses. Since the GPON technology can deliver data, voice, and IP video, it is suitable and popular for fiber to the home (FTTH) transmission. In FTTH application, the passive optical network (PON) based FTTH network is a point-to-multipoint, fiber to the premises network architecture where unpowered optical splitters are used to enable a single optical fiber to serve 32-128 premises. The following text will focus on components and architecture of GPON FTTH access network.

Components of GPON FTTH Access Network

In a GPON FTTH access network, there are three main components: optical line terminal (OLT), optical splitters and optical network terminal (ONT).

Figure 1: Components of GPON FTTH Network

Figure 1: Components of GPON FTTH Network

OLT (Optical Line Terminal)

OLT is a device which serves as the service provider endpoint of a passive optical network. It is an active Ethernet aggregation device that is usually located in a data center or the main equipment room. It is the engine that drives the FTTH system. An OLT converts the optical signals to the electrical signals and presents them to a core Ethernet switch. The OLT replaces multiple layer 2 switches at distribution points. OLT distributing signal is connected with backbone cabling or horizontal cabling through optical splitters, which are connected to the optical network terminal at each work area outlet.

Optical Splitter

The optical splitter splits the power of the signal. That is to say, each fiber link entering the splitter may be split into a given number of fibers leaving the splitter. Usually, three or more levels of fibers correspond to two or more levels of splitters. This enables sharing of each fiber by many users. The passive optical splitter has the characteristics of broad operating wavelength range, low insertion loss and uniformity, minimal dimensions, high reliability, and supporting network survivability and protection policy.

ONT (Optical Network Terminal)

ONT is deployed at customer’s premises. It is connected to the OLT by means of optical fiber and no active elements are present in the link. In GPON, the transceiver in the ONT is the physical connection between the customer premises and the central office OLT.

Architecture of GPON FTTH Network

With a tree topology, GPON maximizes the coverage with minimum network splits, thus reducing optical power. An FTTH access network comprises five areas, which are a core network area, a central office area, a feeder area, a distribution area and a user area/customer premises (see the picture below).

Figure 2: Architecture of GPON FTTH Network

Figure 2: Architecture of GPON FTTH Network

Core Network

The core network includes the internet service provider ISP equipment, PSTN (public switched telephone network, packet switched or the legacy circuit switched) and cable TV provider equipment.

Central Office

The main function of the central office is to host the OLT and ODF (optical distribution frame) and provide the necessary powering. Sometimes it might even include some of the components of the core network.

Feeder Network

The feeder area extends from ODF in the central office (CO) to the distribution points. These points, usually street cabinets, are called fiber distribution terminals (FDTs) where level-1 splitters usually reside. The feeder cable is usually connected as ring topology starting from a GPON port and terminated into another GPON port as shown in the picture above to provide type B protection.

Distribution Network

Distribution cable connects level-1 splitter (inside the FDT) with level-2 splitter. Level-2 splitter is usually hosted in a pole mounted box called fiber access terminal (FAT) usually placed at the entrance of the neighborhood.

User Area

In the user area, drop cables are used to connect the level-2 splitter inside the FAT to the subscriber premises. For ease of maintenance, usually an aerial drop cable is terminated at the entrance of the subscriber home with a terminal box (TB), then an indoor drop cable connects the TB to an access terminal box (ATB) residing inside the home. Finally a patch cord connects the ONT to the ATB.

Summary

From all the above, GPON technology plays an important role in a FTTH network. A GPON-based FTTH network architecture is reliable, scalable, and secure. Since it is a passive network, there are no active components from the CO to the end user, which dramatically minimizes the network maintenance cost and requirements. The GPON-based FTTH is a future-proof solution for providing broadband services.

26.1k

You might also be interested in